CE conformity

  • The CE certification is now based on more than 25 EU directives as of 2020.
  • The CE certificate is a kind of voluntary commitment.
  • The CE mark on a machine and the corresponding signature confirms that this machine was planned, designed and built in accordance with the applicable standards.
  • The CE marking is part of further regulations. These include for instance the Machinery Directive, the Electromagnetic Compatibility (EMC) Directive, the Low Voltage Directive (often referred to as LVD), RoHS substance restrictions and protective equipment etc.

CE conformity is based on a complex risk assessment.

  • Check the intended use of e-chain® and chainflex® cables for instance
  • Analysis of conceivable, foreseeable misuse
  • Determination of relevant and valid standards for the production of chainflex® cables and e-chains®
  • Determination of specific requirements and conditions for the use of chainflex® cables
  • Research of the responsible "notified body", for example, the accreditation body DAkkS (institute for the surveillance of all certification, testing and inspection bodies)
  • (Laboratory) tests of the chainflex® cables and e-chains®
  • Data evaluation
  • Creation of the technical documentation and translation into target languages
  • Creation of the certificate/provision for download
  • Affixing the CE mark

Small sign, big effect

CE