Change Language :

A step by step guide to your required energy chain
igus® offers numerous online tools to quickly configure and order complete energy supply modules. But what if you have no idea where to begin? This step by step guide is to help you go through each step to ensure you have all the information to complete the configurator and get the correct chain at the best price. If you are still not sure what the best options for your application, there is a form for you to complete at the bottom or you can contact one of our experts below.

This step is to identify what services you intend on feeding through the energy chain.

Depending on the length of travel will depend on the best suited energy chain.

This can be looked at 2 ways.

Enviromental factors can have a great impact on the seclection process of the energy chains. Examples such as;

Knowing the bend radius is crucial to prevent kinking and damage to the cables. But what is the bend radius? The bend radius is the maximum radius that a cable will be bent in the application without causing damage to that cable. The image to the right shows the bend that the cables will endure. Different cables have different limitations, so it is vital that you have the correct bend information. Elements for consideration;

There are numerous options of orientation for the energy chains; rotational, horizontal and vertical.

On the majority of energy chains, not just igus® ones, the part numbers can be found on both the side links and cross bars. Click on the orange arrows to expand the image.
Side links can be found along the side of the energy chain and the cross bars run across the width of the chains.

Configure your energy chain using our free tool.
Configure your e-chain®
Find out about our large Chinflex® cable range.
Discover now